Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the parameter need to be check while Selecting Fiber Optic Cable for BMXNRP0200 Module.
Parameters are specified by the cable manufacturer and are based on:
  • The wavelength of the optical signal: 1310 nm in the Quantum EIO optical link
  • the cable index: use graded-index cable only
  • the fiber size:
  • 50/125 μm or 62.5/125 μm
  • 9/125 μm
For most multimode optical cable links, the use of 62.5/125 μm cable is recommended because of its relatively low loss and signal distortion.
  • Select the fiber optic cable that meets the demands of your application. Multiconductor cables are recommended.
Most 62.5/125 μm cables are rated at 1.5 dB loss per km. With a Multiconductor cable, pairs come with an attenuation specification as measured, which is less than 3.5 dB/km.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings