When drive is regenerating, the drive switches on the braking transistor when the value of bus voltage is superior at threshold voltage.
If the value of the bus voltage is inferior at the same threshold, the transistor switches off.
Refer to attached file for voltage value: The threshold is OBR.
Released for: Schneider Electric India