Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which parameters need to be set for Modbus communication on ATV71 drive.
Following parameters are required to program for Modbus communication:
- Do the factory setting of drive.
- Configure [ ACCESS LEVEL] (LAC-) to Expert
- Configure Fr1 to Modbus

- Configuring communication parameters:--
[Modbus Address] : 1 .
[Modbus baud rate]: [19.2 Kbps]
[Modbus format]: [8 E 1]

For modbus run command, you have to use CMD (Logic address 8501) to run the ATV71 drive via Modbus and you will put respectively 16#0006,16#0007 and 16#000F and for frequency setpoint, use the LFR (Logic address 8502).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings