Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How parameter “ACC” works on ATS48 Soft Starter.
ACC parameter is independent from the control mode. It is always a parameter which depends on torque according to time.
If CLP = ON, the torque is linear. If CLP = OFF, the voltage is linear.
Take care because ATS48 is a softstarter and not a drive so the parameter ACC have not the same function.
For instance, if you choose ACC = 30 seconds, it doesn't means that you will start your motor during 30 seconds. In fact, the start duration depends on the load, on the current limitation, on the control mode,
In CLP = ON (torque control mode) if you increase the current limitation ILT, the acceleration time ACC decrease and vice versa. These 2 parameters are linked.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings