Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the voltage inputs rated at for PowerLogic PM8000 series meter ?
Voltage inputs
• Measured voltage: 57 to 400 V L-N / 100 to 690 V L-L (Wye) or 100 to 600 V L-L (Delta or Wye with unearthed neutral)
• Frequency: 50/60 Hz ± 15%, 400 Hz ± 10%
• Overload: 600 V L-N or 1035 V L-L
• Impedance: 5 MΩ
• Measurement category III
• Electromagnetic environmental class: E2
• Mechanical environmental class: M1

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings