Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of BMXERT1604T module supported on Local rack of M580 Standalone CPU.
In a Modicon M580 local drop, the maximum number of BMX ERT 1604T modules depends on the local drop CPU type and the maximum number of Expert channel supported. A BMX ERT 1604T module is counted as 4 expert channels.
Maximum 25 BMXERT1604T module can be configured on M580 Local rack on EIO Network depending on the type of CPU .

For Example:

BMEP581020 = Expert channel supported = 36 /4 = 9 ERT module.
BMEP582020 = Expert channel supported = 72/4  = 18 ERT module.
BMEP582040 = Expert channel supported = 72/4  = 18 ERT module.
BMEP583020 = Expert channel supported = 108/4  = 27 expert modules = Max 25 ERT module + rest other expert modules like counting , Motion module.
BMEP583040 = Expert channel supported = 108/4  = 27 expert modules = Max 25 ERT module + rest other expert modules like counting , Motion module.
BMEP584020 = Expert channel supported = 144/4  = 36 expert modules = Max 25 ERT module + rest other expert modules like counting , Motion module.
BMEP584040 = Expert channel supported = 144/4  = 36 expert modules = Max 25 ERT module + rest other expert modules like counting , Motion module.
BMEP585040= Expert channel supported = 180/4  = 45 expert modules = Max 25 ERT module + rest other expert modules like counting , Motion module.
BMEP586040 = Expert channel supported = 216/4  = 25 expert modules = Max 25 ERT module + rest other expert modules like counting , Motion module.

Refer the attached document for maximum Expert Channel supported with M580 CPU.

Schneider Electric India

Attachment(s)
M580_Expert channel.7z [303.85 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings