Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does SURT20KUXI UPS support modbus RTU ?
Yes, SURT20KUXI UPS does support Modbus RTU by using AP9622 card. if the Customer wants to use the Modbus RTU for monitoring SURT20KUXI UPS, then the following needs to be done:

The customer needs to remove the NMC card from the UPS if he does not want to use the SNMP for monitoring the UPS on the network. There are options available to monitor the UPS via both SNMP and Modbus RTU with additional parts.

The customer needs to purchase AP9622 card + RS232 to RS485 Converter(powered converter).

Install AP9622 card in SURT20KUXI UPS smart slot to configure Modbus, and Modbus RS485 output can be taken from the converter(RS232 to RS485)

NOTE : RTU (remote terminal unit)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings