Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can we set the Output Frequency using the display for SURT15KUXI ?
Kindly follow the below steps to set the frequency for SURT15KUXI using diplay:

1.Click on ‘Enter’ button for Main Menu.
2. Select the ‘Setup’ option from Main Menu and enter on it.
3. Inside the 'Setup'option, select third option ‘System’ and click enter on it.
4. Again enter on the option and select Frequency as per the below options:

Output Frequency Options:

Auto Sensing; 50 Hz; 60 Hz
50 Hz frequency range: 50±3 Hz; 50±0.1 Hz
60 Hz frequency range: 60±3 Hz; 60±0.1 Hz

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings