Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set Low battery state indication in UPS SRC1KI-IN ?
The UPS will emit an audible alarm when the actual run time reaches the limit set by the end user. The audible alarm will emit only when the UPS is working in battery mode. To set low battery Alarm indication to follow below steps
1)Go to the Main menu select 'configuration' press enter
2)Select 'Low battery state indication '  press enter
3)Select option 2 min, 5 min,8 min, 11 min,14 min, 17 min,20 min, 23 min according to your requirement.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings