Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What to do if BR1000G-IN is not powering on ?
Reason for the Problem:

1. The Back-UPS is not connected to utility power.
2. The circuit breaker has been tripped.
3.The internal battery is not connected.
4. The utility input voltage is out of range.

Solution:

1. Ensure that the Back-UPS is securely connected to an utility power outlet.
2.Disconnect non-essential equipment from the Back-UPS. Reset the circuit breaker. Re-connect equipment one item at a time. If the circuit breaker is tripped again, disconnect the device that caused the trip.
3.Connect the battery.
4.Adjust the transfer voltage and sensitivity range.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings