Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What to do if Br1000G-IN is operating on battery power, while connected to utility power ?
Reason for the Problem:

1.The plug has partially pulled out of the wall outlet, the wall outlet is no longer receiving utility power, or the circuit breaker has been tripped.
2. The Back-UPS is performing an automatic self test.
3. The utility input voltage is out of range, the frequency is out of range, or the waveform is distorted.

Solution:

1.Ensure that the plug is fully inserted into the wall outlet. Ensure that the wall outlet is receiving utility power by checking it with another device.
2.Adjust the transfer voltage and sensitivity range.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings