Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we need to be present physically at the device for the firmware upgrade or can it be managed remotely as well?
The firmware upgrade can be done remotely on the network online. Make sure FTP port is opened for the rPDU IP address and reachable via FTP.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings