Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
For TM221 controller, is there a method to create a clone of the application in SD card when the application has application protection enabled
In case of application is password protected inside M221, Clone function is blocked and there is no other way to clone application from controller.

What user can do is he can clone the application from the EcoStruxure Machine Expert Basic and onwards but it is must to have a project.
If project back-up is there then open the project. Go to the Commissoning => Controller Management => Controller Memory Management => Action = Create controller image.
Save this image file to the directory on system of PC or to Controller SD card whichever is feasible.
Check the box, Include firmware if firmware is to be cloned.
By this way image is copied and later it can be copied to the other controller.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings