Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reset KWh in PM8240 meter.
In PM8240 , the device framework is the same as that we can see on the ION7650 and similar devices (i.e. the ION8600, 8650, 8800, 7600 etc.) and these devices reset to zero at the threshold that is set.

By default, the framework resets to zero at the default threshold which is 10 000 000 kWh.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings