Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How Immediate Access to an Ethernet Remote I/O Drop can be performed with Quantum Ethernet I/O.
An IU_ERIO function block can be used to updates Ethernet remote I/O drop input and output modules with an optimal response time. The Ethernet remote I/O drop inputs and outputs are updated during the MAST task.
Call this function block in a MAST task. It can be called more than once in a task.

NOTE: To maintain system performance, we recommend that you use no more than 10 executions of the IU_ERIO block during a single MAST task.

Refer the attached file for help on IU_ERIO function block.

Schneider Electric India

Attachment(s)
IU_ERIO.pdf [125.59 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings