Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the settings to use webserver on ATV600 series.
(1) [Enable Web Services] (EWEE)
This parameter is used to manage the embedded Ethernet Web services.
This parameter is accessible via [My preferences] (MYP-) menu and [Webserver] (WbS-) submenu.
In factory setting,it is enabled (i.e.Yes)

(2) Go to [Embedded Ethernet Configuration] EtE- Menu
Program [IP Mode Ether. Embd] to Fixed address.
Then enter IP address : example :10.5.8.9
Subnet mask to 255.255.255.0

(3) Then configure the PC LAN IP to the same domain
For this go to Local Area connection of your PC
Select Internet Protocol Version 4(TCP/IPv4) and go to properties
And select “ Use the following IP address” then enter IP address:for example : 10.5.8.15
And Subnet mask to 255.255.255.0 then click O.K.

(4) The webserver can be accessed from standard browsers like Internet Explorer, chrome.
First connect the computer to the drive by typing http:// followed by the drive IP address.
https:// 10.5.8.9
By default the user name is ADMIN and the password will appear  via [My preferences] (MYP-) menu and [Webserver] (WbS-) submenu when Ethernet Cable is connected
Once connected, the webserver home page is displayed.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings