Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why the response time of MX/XF COM Coil increased when compared to standard coils.
MX/XF COM Coils are power supply permanently and  to operate need :

* an order from the BCM or

* from the local electrical close : "you have only to switch off the contact during 5ms" to see the MX/XF operating

or

* Remote close : "you have  to switch off the contact during 50ms" to see the MX/XF operating" it is why we say that the response time between a MX/XF COM is increased !!

This increase of time is due to treatment of the informations by the COMM COILS.

The standard Coils operate only if you supply it, so it have a small response time



Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings