Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it recommended to use 2NO/2NC LC1D188** for changeover application.
2NO/2NC LC1D188** contactors are design for 2 speed motor applications. Source change over system must be constructed using 2 different contactors mechanically and electrically interlocked to avoid any issue during source change over operation

So it is not recommended to use LC1D188** contactor for changeover application because using 2NO/2NC contactor in source change over application will lead to contactor issue

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings