Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of 3 way selector switch with 2 number NC contact and padlock at center.

Part number of 3 way selector switch with 2 number NC contact and padlock at center : ZB4BJ593+ ZB4BZ104

Where ZB4BJ593 is black selector switch head Ø22 3-position spring return to centre, Black long handle and Padlockable at center only.

ZB4BZ104 is complete body/contact assembly with 2NC.

Refer to attachment for the data sheet of ZB4BJ593 & ZB4BZ104.

Schneider Electric India

Attachment(s)
Data sheet.zip [201.24 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings