Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is CLF fault on the ATS48 Soft Starter.

CLF is Control Line Failure.
• The ATS48 monitors the control voltage via the 2 terminals (CL1-CL2) on the 'control unit'.
• This fault is encountered very infrequently as it is usually transient. The voltage must rise again in order for the switch mode power supply to be present during operation CLF fault trip threshold:
• Voltage less than approx. 40% of 220 V for the ATS48…Q (threshold = 88 V).
• Voltage less than approx. 40% of 110 V for the ATS48…Y (threshold = 44 V).

Probable causes:
• Loss of the line voltage for at least 200 ms on terminals CL1-CL2.
• Voltage thresholds exceeded.

Remedies:
• Check the value of the voltage at terminals CL1-CL2: if the voltage is within the tolerances, replace the power board.
• Check the quality of the line supply.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings