Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the power factor for ATV212 drive range.
Power factor at 100% load: -
PF = Cos Phi(1)/SQR(1+THD²) where Cos Phi(1) is from the fundamental current.
PF = 1/SQR(1+THD²) because Cos Phi is closed to 1.
For THDi of each rating at 100% load, Refer to attached document.
Then it is possible to estimate the Power Factor of the ATV212:
For Example:
ATV 212HD22N4(22KW)
THDi=30.7 (see attached File1)
So, estimated power factor = 1/SQR(1+ .307²) = 0.95
Same way, it is possible to calculate power factor for other part number also.

Schneider Electric India

Attachment(s)
THDi_ATV212.zip [183.82 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings