Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the climatic withstand conditions for Compact NSXm circuit breakers.
The Compact NSXm circuit breakers have successfully passed the tests defined by the following standards for extreme atmospheric conditions.

Dry cold and dry heat:
-> IEC 60068-2-1: dry cold at -55 °C
-> IEC 60068-2-2: dry heat at +85 °C.

Damp heat (tropicalization)
-> IEC 60068-2-30: damp heat (temperature + 55 °C and relative humidity of 95 %).
-> IEC 60068-2-52: severity 2 - Cycling salt mist.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings