Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to set the sensitivity in Back-UPS BR1000G-IN / BR1500G-IN ?
Important Note:
a. Ensure that the Back-UPS is Off but connected to utility power.
b. Ensure that the Load's are not connected with the Back-UPS

Step 1 : Press and hold the Power button until the Load graph starts flashing sequentially, This indicates that the unit is in Programming mode.
Step 2 : Press the Power button again immediately to rotate through the menu options.
There are totally 5 bars in the Load Graph. If first load graph bar flashes , Unit is set to Low sensitivity - 150-300 Vac
If First three load graph bar flashes , Unit is set to Medium sensitivity (Default) - 170-294 Vac
If All the load graph bar flashes , Unit is set to High sensitivity - 170-288 Vac

Step 3 : Stop at selected Sensitivity .The Back-UPS will beep to confirm the selection.

Please find the Video

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings