Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot access the command line interface remotely of NMC card AP9631 ?
Possible cause & Solution:
• Make sure you are using the correct access method, Telnet or Secure SHell (SSH). An Administrator can enable these access methods.
By default, Telnet is enabled. Enabling SSH automatically disables Telnet.
• For SSH, the NMC may be creating a host key. The NMC can take up to one minute to create the host key, and SSH is inaccessible for that time.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings