Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Not able to ping IP address assigned to NMC card AP9630 ?
Solution: If the NMC’s Status LED is green, try to ping another node on the same network segment as the NMC. If that does not work, it is not a problem with
the NMC. If the Status LED is not green, or if the ping test succeeds, perform the following checks:
• Verify that the NMC is properly seated in the UPS.
• Verify all network connections.
• Verify the IP addresses of the NMC and the NMS.
• If the NMS is on a different physical network (or subnetwork) from the NMC, verify the IP address of the default gateway (or router).
• Verify the number of subnet bits for the NMC’s subnet mask.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings