Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Whether different Class CT's can be used for Sepam 64REF protection.
CT requirement for any application depends on some factors knee-point voltage accuracy-limit factor

64REF can be of Low Impedance type & High Impedance type

1) 64 REF-Low Impedance - Phase CT & Neutral CT can be of different class.For Example : Class X for Neutral CT & Class 5P10 for Phase CT ;
Different Class CT's can be used subject to they should fulfill the values of Knee point voltage & other recommended parameters.

2) 64 REF-High Impedance - CT's of Different Class type should not be used.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings