Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is GENIO and GENANAIO modules in Modicon Quantum range.
Go through the description as below:

GENANAIO:  It is a generic analog input/output module

GENIO: It is a generic digital input/output modules.

These module can be used only with partner modules (Spectrum Control , Niobrara,Prosoft etc.).
All the specific parameters to be entered for correct use of a given module are provided by the company that manufactures this module(personality, number of input/output words, BCD I/O, etc.).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings