Real time clock can be managed remotely by using System word %SW49 to %SW53 which is for Real-time clock function. to write the value from program or GUI, %S50 bit should be set as 1 using unity Pro software.
These words are managed by the system when the bit %S50 is set to 0.
These words can be written by the user program or by the terminal when the bit %S50 is set to 1.
These words are managed by the system when the bit %S50 is set to 0.
These words can be written by the user program or by the terminal when the bit %S50 is set to 1.
Released for: Schneider Electric India