Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Process to achieve Time sync in PM8240
Time Sync can be performed using option Clock > TimeZone > Cl1 Clock Source.
Clock source have three options which be configured as per the site network/architecture.
Options are:
• Internal: the meter’s internal clock.
• Line frequency: the frequency of the measured power system as the clock source.
• COMM: the meter’s communication port (used by the GPS time sync source).

Schneider Electric India

Attachment(s)
timezone.JPG.jpg [38.23 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings