Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do MiCOM P132 relays conforms to Electrical Fast Transient or Burst Requirements Test.
The MiCOM P132 relays conforms to Electrical Fast Transient or Burst Requirements Test as per EN 61000-4‑4 and IEC 60255‑22‑4, severity levels 3 and 4.
● Rise time of one pulse: 5 ns.
● Impulse duration (50% value): 50 ns.
● Amplitude: 2 kV / 1 kV or 4 kV / 2 kV.
● Burst duration:15 ms.
● Burst period: 300 ms.
● Burst frequency: 5 kHz.
● Source impedance: 50 Ω.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings