Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does X80 discrete IO modules have short circuit protection in-built.
Built-in protection is available for X80 discrete IO modules. However use fast blow fuse on output field terminal of appropriate rating. Below are the built in protections available in X80 DO modules:

against over voltage =  Yes, by Transil diode
against inversions =  Yes, by inverted diode
against short-circuits and overloads =  Yes, by current limiter and electric circuit-breaker 1.5 In < Id < 2 In

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings