Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Active Power (LAP) value is not displayed over ATS48 soft starter display and the connection is starter wired to the motor delta terminals. What is the reason.
Such kind of behavior can appears inside delta wiring when connection is not correctly done , So cos=0 (angle between voltage and current is not on the right direction) ,So ,active power is equal to 0 kW (due to cos=0).It is important to check that ATS48 follow the starter wired to the motor delta terminals (Motor winding position to right soft starter output terminal and input) wiring. Refer to attached document.

Schneider Electric India

Attachment(s)
Starter wired to the motor delta terminals.pdf [79.49 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings