Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Relay R3 configured to tAI; When Relay R3 will be activated on ATS48 Soft Starter.
When you configure R3 = tAI (Motor Thermal Alarm): this relay will be activated when the tHr (motor thermal state) is > 110%. in this case ATS48 will not trip in fault. the state of R3 will be deactivated if tHr <110%.
Note:  A thermal fault stops the motor if it exceeds the critical temperature rise threshold (motor thermal state >125%).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings