Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any document about % THDv for ATV630 drives.
The THDv value cannot be specified by the drive manufacturer. The THDv value depends on the existing mains topology (mains short circuit capability, transformer impedance, …) at the customer side.
So, for the THDv we don’t have values as the it is a result of the THDi and the mains topology.
We have a harmonic simulation tool; please see below link;

http://10.129.134.120/default.aspx

With the above said tool you can simulate the THDi and THDv values for ATV630 drives.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings