Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How ATV212 drives measure the Line voltage.
ATV212 drive does not measure directly the line voltage. it measures only the DC bus voltage.
Drive estimates Line voltage (FE04); For Example:  if you measure the DC bus voltage = 301 Vdc.
Then DC bus voltage = 1.414 x Line voltage
Line voltage =DC bus voltage/1.414 = 301/1.414 = 212.8 V
The drive estimates that the line voltage is closed to 213Vac.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings