Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
As AS-P/B has two On-board Ethernet ports on it so can they be inter-connected.
The second Ethernet port is currently not meant to be used to connect to another AS-P/B.
The two Ethernet ports are connected to a built-in Ethernet switch. One port should be connected to the site network. The other port can be used to connect a single WorkStation or WebStation, a Modbus TCP unit, or a BACnet/IP device, but not another SmartStruxure server.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings