Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to have motor nominal torque at 0 RPM speed in ATV320 drives
To have torque at 0 RPM speed in ATV320 configure: Continuous fluxing or Continuous DC injection functions.
But the continuous fluxing will offer very small torque (no really torque).
DC injection could be a little bit better because user can select the current level to inject but it could not be of order motor nominal torque.
There is no better solution in open loop vector control mode for ATV320 drives.
Possible solution is to connect encoder and operate drive in closed loop - Flux Verctor Control mode. This option is not applicable in case using ATV320 family drives rather
user can switch to ATV71 / ATV9xx process family drives.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings