Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set the Low Load Warning Threshold for AP4424 Switch.
The default Low Load Warning Threshold is 0 Amps, which disables the warning alarm. A 2-Amp detection threshold indicates that a circuit breaker may have tripped and activates a warning alarm. ï With a setting of 0 Amps for the Low Load Warning Threshold, the Web interface will not indicate that a circuit breaker may have tripped.
1. Select the Unit tab from the navigation menu, then select load, under Configuration in the left navigation menu.
2. Set the Low Load Warning Threshold for each bank to 2 Amps.
3. Click Apply to save your changes or Cancel to exit without saving the changes."

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings