Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I get the Default IP Address of BMX NOR0200H Module.
Default IP Address of BMXNOR0200H Module can be get from it's MAC Address.

The default IP address format is 84.x.y.z:
  • 84: a fixed value
  • x.y.z: The last three fields in the default IP address correspond to the decimal equivalents of the last three bytes in the MAC address.
Example:

For example a device with 00-00-53-12-01-C4 MAC address has the following default IP address: 84.18.1.196 (12 hex = 18 dec, 01 hex = 1 dec, C4 hex = 196 dec)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings