Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I create a SCL file for all the signals, If I do not have Easergy P3
First create an off-line setting file, make sure you select Ethernet port(s) in hardware selection and IEC61850 as Ethernet port protocol.
In next step select all signals used to “In use” under Communication/data maps. Then select tool icon and “Export ICD/SCL file…”.
Before generation you need to define if RCB names should include indexes (typically selected) and if the file should be in Ed.1 or
Ed.2 format. If Edition 2 extensions are selected the file will be created in Ed.2 format, otherwise Ed.1 format. When saving the file there is the
possibility to save the format as .icd, .iid or .cid.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings