Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure Port sniffing support in Vamp 50 and Vamp 200 series.
With the new Ethernet interface it is possible to monitor all packets received and transmitted by VAMP relay. This so called Sniffer mode can be enabled under ETHERNET
PORT group on PROTOCOL CONFIGURATION tab in Vampset. Sniffer port is always set to EthPort2 and cannot be changed, thus an external device used for network traffic monitoring should be connected to Port2.

Remember that Sniffer mode cannot be enabled if Storm protection logic is already enabled on at least one port.

Refer the snapshot attached.

Schneider Electric India

Attachment(s)
vamp sniffer port.JPG.jpg [29.25 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings