Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can Factory Supplied Report be edited in EcoStruxure Building Operation.
Factory Supplied Report can be edited using the MS Report Builder which is a separately downloadable part of Microsoft SQL Server 2008 and SQL Server 2012, and provides the facility to create, modify, and deploy your own reports to the Reports Server, based on selected parts of the EcoStruxure Building Operation database. Below is the basic procedure.
- In MS Report Builder, click the main menu button, and then click the Options button.
- In the Use this report server box , type http://localhost/reportserver_SQLEXPRESS .
- Click OK .
- Click the main menu button and then click Open .
- Select the folder that contains the factory supplied report that you want to edit.
- Select your factory supplied report.
- Click Open .
- Right click the area of the report that you want to edit, and then select the properties command.
- Edit the properties.
- Click OK .
- Save your edited report to the required location.

You can now synchronize your edited report with WebReports.
For more detailed information about the Report Builder third-party software, please refer to the Microsoft Report Builder Online Help.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings