Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the purpose of “Assignment of relay R1 to isolating relay (r1I)” on ATS48 Soft Starter.
Assignment of relay R1 to isolating relay (r1I); Relay R1 is designed to control the line contactor on the basis of the RUN and STOP commands and to indicate faults. Relay R1 is activated by a RUN command. It is deactivated at the end of deceleration or when the motor switches to freewheel mode after a STOP command. It is also deactivated when a fault occurs.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings