Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use High resolution speed reference on ATV312 drive.
To send reference via communication like 0 to 100%, it is possible to use the high-resolution mode. We can change the precision of LFR (send by communication) to have high resolution.

To activate the high-resolution mode, the bit 9 of CMI must be set to 1.

bit 9 = 1: High resolution (references, output speed and ouput frequency in 32767 points for 600 Hz)
600/32767 =0.0183

600 Hz= 32767
1 Hz= 32767/600= 54.611
50 HZ =50x54.611=2730.55

LFR=>100=> the drive will run at 1.8 Hz
LFR=>1000 => the drive will run at 18.3 Hz
LFR=>2000=> the drive will run at 36.6 Hz
LFR=>2500=> the drive will run at 45.8 Hz
LFR=>2600=> the drive will run at 47.6 Hz

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings