Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the nLP on ATS48 Soft Starter.
The nLP state of the ATS48 is not the state of loss of input phase.
And the nLP occurs if there are least 2 lost phases.

The loss of input phase is PHF state.
And the triggering of PHF only occurs with the run command and one or more phases are lost.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings