Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the specific limitation with BMECXM0100 module.
When you use a BMECXM module on the Modicon M580, observe these limits:
1. Each BMECXM module can manage a maximum of 63 CANopen slaves.
2. The size of the configuration file (.prm) of each BMECXM module is limited to 64 Kb maximum.
3. Each BMECXM module on the Ethernet bus communicates with the CPU. They are in the same network. Transparency is thus provided from the CPU or any PC connected on the same subnet up to the BMECXM module.
NOTE: No communication is possible between two BMECXM modules.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings