Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of "BS" LED on BMECXM0100 module.
BS led is for bus status. Details as in below indicate the consequences of different Led patterns:

LED Off:
-  Module is not configured, or
-  Module is waiting for IP address from DHCP.
Green:
On  : All EtherNet/IP connections are established.
Flashing:  The module has an IP address, but there is no EtherNet/IP connection.
Blinking:  The power on self-test is in progress.
Red:
On:  There is a duplicate IP address.
Flashing:  At least one EtherNet/IP connection is lost. The LED flashes until the connection is re-established or the module is reset.
Yellow Blinking:  The loading of the firmware is in progress.


Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings