Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the use of Modicon IEC 61850 Configuration Tool in unity pro.
The IEC 61850 configuration interface in Unity Pro is the exclusive tool for configuring IEC 61850-
based properties of the BMENOP0300 module.
Use the Modicon IEC 61850 Configuration Tool to perform the following tasks:
1. Configure the BMENOP0300 module as an IEC 61850 server or client
2. Configure the IP address settings for the module
3. Configure Ethernet services for the module, including:
a. RSTP
b. SNTP
c. SNMP
d. Security
e. Switch settings (baud rates for the Ethernet ports)
f. Syslog

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings