Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the use of "NI" parameter in GOOSE Subscriber section in Easergy P3
Index of GOOSE Network Input for the receive GOOSE data point (can be binary or analog). Binary NIs can be used as inputs for
the user-defined logic blocks or as control inputs in the other functions of the relay (e.g. the output matrix).
Analog NIs (virtual analog inputs) can be used as coupling in programmable stages.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings