Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is Bridge priority parameter in RSTP settings in Easergy P3
Root bridge identifier, taken into account during building and adjusting the spanning tree structure inside the network.
The relay with the best bridge priority (lowest value) becomes an RSTP root device for that network. If priorities of two or more relays are equal,
the relay with the lowest MAC address is chosen as a root.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings